DBS Scala2 Internal Launching

15/04/2016

DBS Scala2 Internal Launching

On 1 April, the SCALA2 domestic booster system from Grundfos is released internally in Grundfos Indonesia.

Few days before launching, all employees were curious about the sticker that was placed in Grundfos lobby which says “ Waiting on April 1 its not April Mop ”.  Now the curiosity answered by the launching of the SCALA2 domestic booster system.  SCALA2 system comes with intelligent pump control, it means the pump will automatically adjusts operation to deliver the water pressure that you prefer. The integrated sensor detects if the inlet pressure varies or if there are several taps open and immediately tells the pump to boost the pressure. It happens so fast that you will not notice any change in your water pressure at all. The SCALA2 can keep pressure high in buildings with up to the 3rd floor, and it is compact enough to fit into a kitchen cupboard. The water-cooled pump also runs at a low noise level, making it sought after in private homes. Opened by Domestic Building Service Manager F. Chandradinata, this launching event features a wide range of marketing material such as demos SCALA2 running, cutting product, hologram displays, posters and floor column. In addition, participant also received gimmicks, a temporary tattoo of SCALA2 and Grundfos small notes/agenda." Hopely we can Increase sales with this product", says Gert Borrits, Managing Director of Grundfos Indonesia." I was very curious when viewing floor stickers, what is going to happen on the 1st of April ? I thought there will be April mop, but it turned out to be real. Very creative and what a cool pump it is !!!..." There is a chip inside the pump ", says Andri, GAS Customer service.





    Facebook Twitter LinkedIn Technorati