SP Campaign First Road Show in Indonesia

19/11/2014

Mr. Tegoeh with One of the Dealer

As part of activities to improve and maintain market share Grundfos SP Pumps which is one of the backbone of Grundfos Indonesia's sales, starting by end of August 2014, Water Utility segment will hold a SP Campaign road show in several major cities in Indonesia.

In addition to increase the sales of SP Pump, the event is also aim to build a better relation with the end customer, especially professional well driller, and also to give updated information about the latest Grundfos’ products to the public.

The first major city that starts off theSP Campaign was Bandung. The event was held on August 26 in Hotel Horizon Bandung. It started from 6 PM. About 50 to 60 well driller attended the event from 30 companies that are located in West Java. The event end successfully as planned.

On the same occasion, Mr. Tegoeh Boediono, Segment Manager Water Utility launch promotion programs as a part of marketing strategy for hard-selling SP Pump. The SP Campaign in Bandung was fully supported by the management of Grundfos’ Pump sales and Grundfos Authorized Dealer in West Java.





    Facebook Twitter LinkedIn Technorati