SQ Surabaya

20/11/2014

SQ DBS in Surabaya

SQ are back again. Now, they came to Surabaya.

For increasing sales and product knowledge to market, DBS team of PT Grundfos Pompa continued their re-launching product of SQ Submersible Pump for the fourth time. This event was held in Surabaya at Hotel Santika Premiere Surabaya, on Friday and Saturday, 19 - 20 September 2014.

Based on the positioning of SQ Pump, which is modern and high-tech, DBS choose the modern technology concept for this event. It can be seen by a Female DJ performance and also the demo running of SQ Pump.

This event which was held for 2 days are had a difference audience. First day on 19 September are pointed to POS which was attended by around 42 people, and the second day, 20 September 2014 are pointed for Professional installer which was attended by around 37 people.
This time they proven their succesfull event by reach around 40 unit SQ Pump order on the first day, and 5 unit SQ Pump on the second day. This number will likely continue to grow even after the event.

“The advantages of SQ Pump among others are capable of operating at a voltage of 150V up to 315V, has a vacancy protection of water (dry running protection), extremely light weight, made of high quality stainless steel that is resistant to corrosion, only 3 inches in diameter and easy to install.” Said Mr. F. Chandradinata, our DBS Business Unit Manager of PT. Grundfos Pompa while giving a speech at the event.

For next destination we will be ready for Yogyakarta, Solo, and Semarang. See you soon guys!





    Facebook Twitter LinkedIn Technorati