Milk reception

Overview

Overview

Milk reception

Grundfos' range of sanitary pumps is ideal in milk reception applications where it is important to efficiently transport the milk from one tank to the next – or from the milk tanker into the dairy.

In by far the majority of dairies the milk is transported from the milk tanker into the tanks using a single-stage centrifugal pump. If higher pressure is required, a multi-stage pump is available. In order to completely empty the milk tanker, a single-stage self-priming pump, creating vacuum on its own, can be supplied.

Cleaning: All Grundfos’ sanitary pumps are CIP-compatible, allowing tanks, pipes and process lines to be efficiently cleaned without having to dismantle the equipment. A CIP-system can also be applied to the milk tanker to allow easy and 100% reliable cleaning of the inside of the tank. Every CIP-system is followed by a single-stage self-priming pump, that will efficiently remove every last drop of detergent in tanks and pipes.

ChallengeSolution
Maximum hygiene is essential in all dairies.All Grundfos' sanitary pumps are CIP- compatible, allowing tanks, pipes and process lines to be efficiently cleaned without having to dismantle the equipment. Precise dosing pumps speed up the CIP-process by adding only the necessary detergent, consequently reducing the flushing of the system. Every CIP- system is followed by a single-stage self-priming pump that removes every last drop of detergent in tanks and pipes by circulating rinsing water.

Important notes

  • Grundfos’ sanitary pumps carry the EHEDG certificate. Certain models also carry the 3A certificate.
  • Choose SiC/SiC mechanical shaft seals if oxidizing disinfection agents liberate bacteria.

 





    Facebook Twitter LinkedIn Technorati
Related products