Proportional pressure, calculated - control mode

Proportional pressure is used in circulation systems with a pipe system with low pressure loss and control valves to generate a variable flow.

Constant pressure is used in circulation systems with a pipe system with low pressure drop and control valves to generate a variable flow. The pressure drop in the control valves is lower than 50% of the total pressure drop.

  • Heating systems with 2-way valves
  • Air-con system with 2-way valves




    Facebook Twitter LinkedIn Technorati